CAP#.EDGE
Description
Selects which edge of the trigger input to use.
The trigger source is monitored for either a rising, falling, or either edge. When one of these edges is detected the position or time is captured. This setting is always used irrespective of the precondition configuration.
Examples
Usage
1: Rising edge (default)
2: Falling edge
3: Rising or falling edge
Code
-->CAP1.EDGE 1 -->
Context
For more information please refer to Capture.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type |
Read/Write |
| Units |
N/A |
| Range |
1 to 3 |
| Default Value |
1 |
| Data Type |
Integer |
| Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Related Topics
Capture